FlatteningAndFormingBuilderExDistortionMap Enumeration¶
NXOpen.Features.FlatteningAndFormingBuilderEx.DistortionMap is an alias for NXOpen.Features.FlatteningAndFormingBuilderExDistortionMap
-
class
NXOpen.Features.
FlatteningAndFormingBuilderExDistortionMap
¶ Bases:
object
Distortion Map options. The options provides ability to display a distortion map on the source faces.
Enum Members
Enum Member Enum Member Description NotSet No distortion map Length Distortion of length Area Distortion of area Angle Shear distortion of U/V directions -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-