FlatPatternObjectDataGeneral_Struct Struct¶
NXOpen.Features.FlatPattern.ObjectDataGeneral is an alias for NXOpen.Features.FlatPatternObjectDataGeneral_Struct
-
class
NXOpen.Features.
FlatPatternObjectDataGeneral_Struct
¶ Bases:
object
Structure used to return data about objects in the flat pattern.
This structure is for points whose associativities are not covered by the other types, which are returned as tagged objects. Used for the added geometry objects. . Constructor: NXOpen.Features.FlatPattern.ObjectDataGeneral()
Fields¶
Field | Description |
---|---|
FlatPatternObject | Object in the flat pattern |
FlatSolidObject | Corresponding object on the flat solid |
FormedBodyObject | Corresponding object on the formed body |
FlatPatternObject¶
-
FlatPatternObjectDataGeneral_Struct.
FlatPatternObject
¶ Object in the flat pattern
-------------------------------------
Field Value Type:
NXOpen.TaggedObject
FlatSolidObject¶
-
FlatPatternObjectDataGeneral_Struct.
FlatSolidObject
¶ Corresponding object on the flat solid
-------------------------------------
Field Value Type:
NXOpen.TaggedObject
FormedBodyObject¶
-
FlatPatternObjectDataGeneral_Struct.
FormedBodyObject
¶ Corresponding object on the formed body
-------------------------------------
Field Value Type:
NXOpen.TaggedObject