FitSurfaceBuilderTargetType Enumeration

NXOpen.Features.FitSurfaceBuilder.TargetType is an alias for NXOpen.Features.FitSurfaceBuilderTargetType

class NXOpen.Features.FitSurfaceBuilderTargetType

Bases: object

Target type provides the ability to specify a object or a color coded region as the target

Enum Members

Enum Member Enum Member Description
Object This option will select the entire object
ColorRegion
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.