FitCurveBuilderTargetSourceTypes Enumeration¶
NXOpen.Features.FitCurveBuilder.TargetSourceTypes is an alias for NXOpen.Features.FitCurveBuilderTargetSourceTypes
-
class
NXOpen.Features.
FitCurveBuilderTargetSourceTypes
¶ Bases:
object
Fitting target types
Enum Members
Enum Member Enum Member Description Infer Infer target from selection SpecifiedPoints Specified points ChainedPoints Chain using one or two points Curve Curve Face Face FacetBody Facet body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-