FeatureReferencesBuilder Class¶
-
class
NXOpen.Features.
FeatureReferencesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.FeatureReferencesBuilder
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
AutomaticMatch | This function can perform two automatic feature reference matching operations based on: 1. |
GetMatchedReferences | Returns the MatchedReference Builders |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AutomaticMatch¶
-
FeatureReferencesBuilder.
AutomaticMatch
¶ This function can perform two automatic feature reference matching operations based on: 1.
other reference matches; 2. parent names if match_based_on_name is true.
Signature
AutomaticMatch(matchBasedOnName)
Parameters: matchBasedOnName (bool) – match by name or not New in version NX6.0.0.
License requirements: None.
GetMatchedReferences¶
-
FeatureReferencesBuilder.
GetMatchedReferences
¶ Returns the MatchedReference Builders
Signature
GetMatchedReferences()
Returns: Return type: list of NXOpen.Features.MatchedReferenceBuilder
New in version NX6.0.0.
License requirements: None.
Validate¶
-
FeatureReferencesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.