FeatureBooleanType Enumeration¶
NXOpen.Features.Feature.BooleanType is an alias for NXOpen.Features.FeatureBooleanType
-
class
NXOpen.Features.
FeatureBooleanType
¶ Bases:
object
Boolean operation type.
Enum Members
Enum Member Enum Member Description Create Create Unite Unite Subtract Subtract Intersect Intersect EmbossNormalSide Emboss, keep tool on normal side of sheet EmbossOppositeNormalSide Emboss, keep tool opposite of normal side of sheet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-