FaceBlendBuilderWidthMethod Enumeration¶
NXOpen.Features.FaceBlendBuilder.WidthMethod is an alias for NXOpen.Features.FaceBlendBuilderWidthMethod
-
class
NXOpen.Features.
FaceBlendBuilderWidthMethod
¶ Bases:
object
This enum represents the Face Blend width method, it is added in NX10 for two face blend
Enum Members
Enum Member Enum Member Description NaturallyVarying Naturally Varying ForcedConstant Forced Constant TwoConstraintCurves Two Constraint Curves -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-