FaceBlendBuilderTrimmingMethod Enumeration¶
NXOpen.Features.FaceBlendBuilder.TrimmingMethod is an alias for NXOpen.Features.FaceBlendBuilderTrimmingMethod
-
class
NXOpen.Features.
FaceBlendBuilderTrimmingMethod
¶ Bases:
object
This enum represents the Trimming options for Face Blend
Enum Members
Enum Member Enum Member Description ToAllFaces Trim to all faces Short Trim short Long Trim long NotSet No trim -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-