FaceBlendBuilderDefiningType Enumeration¶
NXOpen.Features.FaceBlendBuilder.DefiningType is an alias for NXOpen.Features.FaceBlendBuilderDefiningType
-
class
NXOpen.Features.
FaceBlendBuilderDefiningType
¶ Bases:
object
This enum represents the Face Blend defining type, it is added in NX75 for new three face blend
Enum Members
Enum Member Enum Member Description BlendTwoFace this is for normal two face blend BlendThreeFace this is form new three face blend BlendFromEdges -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-