FaceBlendBuilderCrossSectionOption Enumeration¶
NXOpen.Features.FaceBlendBuilder.CrossSectionOption is an alias for NXOpen.Features.FaceBlendBuilderCrossSectionOption
-
class
NXOpen.Features.
FaceBlendBuilderCrossSectionOption
¶ Bases:
object
This enum represents the Cross section types
Enum Members
Enum Member Enum Member Description Circular Conic this means tangent continuous asymmetric conic type ConicSymmetric this means tangent continuous symmetric conic type CurvatureSymmetric this means curvature continuous symmetric conic type CurvatureAsymmetric this means curvature continuous asymmetric conic type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-