ExtensionBuilderTypes Enumeration

NXOpen.Features.ExtensionBuilder.Types is an alias for NXOpen.Features.ExtensionBuilderTypes

class NXOpen.Features.ExtensionBuilderTypes

Bases: object

The part of the face to extend.

Enum Members

Enum Member Enum Member Description
Edge
Corner
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.