ExtendSheetBuilderSideEdgeShape Enumeration

NXOpen.Features.ExtendSheetBuilder.SideEdgeShape is an alias for NXOpen.Features.ExtendSheetBuilderSideEdgeShape

class NXOpen.Features.ExtendSheetBuilderSideEdgeShape

Bases: object

Determines the path of the extension

Enum Members

Enum Member Enum Member Description
Automatic
Tangent
Orthogonal
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.