EmbossRegionConvexityOption Enumeration

NXOpen.Features.EmbossRegion.ConvexityOption is an alias for NXOpen.Features.EmbossRegionConvexityOption

class NXOpen.Features.EmbossRegionConvexityOption

Bases: object

Describes whether the emboss geometry is above the target(“Pad”) or below the target(“Pocket”), or both(“Mixed”).

Enum Members

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.