EmbossProjectionProjectionOption Enumeration¶
NXOpen.Features.EmbossProjection.ProjectionOption is an alias for NXOpen.Features.EmbossProjectionProjectionOption
-
class
NXOpen.Features.
EmbossProjectionProjectionOption
¶ Bases:
object
Describes the geometry for projection
Enum Members
Enum Member Enum Member Description Endcap Indicates the geometry is End-Cap. Target Indicates the geometry is target. Face Indicates the geometries are selected faces. Plane Indicates the geometry is datum plane. NotSet Indicates no geometry. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-