EmbossLimitEndcapMethod Enumeration¶
NXOpen.Features.EmbossLimit.EndcapMethod is an alias for NXOpen.Features.EmbossLimitEndcapMethod
-
class
NXOpen.Features.
EmbossLimitEndcapMethod
¶ Bases:
object
Describes the method that can be applied to the selected geometry to define the End-Cap.
Enum Members
Enum Member Enum Member Description Translation Indicates End-Cap geometry is a translation along a user controlled vector. OffsetExact Indicates End-Cap geometry is formulated as an exact offset of the selected End-Cap geometry. Default creation. OffsetApproximation Indicates End-Cap geometry is formulated as an approximate offset of the selected End-Cap geometry NotSet Indicates End-Cap geometry is formulated by the selected geometry without displacement. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-