EmbedManagerBuilderTaskTypes Enumeration¶
NXOpen.Features.EmbedManagerBuilder.TaskTypes is an alias for NXOpen.Features.EmbedManagerBuilderTaskTypes
-
class
NXOpen.Features.
EmbedManagerBuilderTaskTypes
¶ Bases:
object
The task to perform on the file.
Enum Members
Enum Member Enum Member Description Embed Embed operating system file in part. Replace Replace the existing embedded file. Rename Rename the existing embedded file. Delete Delete the existing embedded file. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-