EmbedManagerBuilderLocationTypes Enumeration¶
NXOpen.Features.EmbedManagerBuilder.LocationTypes is an alias for NXOpen.Features.EmbedManagerBuilderLocationTypes
-
class
NXOpen.Features.
EmbedManagerBuilderLocationTypes
¶ Bases:
object
The option to specify where the file exists.
Enum Members
Enum Member Enum Member Description OperatingSystem File exists on the native OS. Teamcenter File exists in Teamcenter. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-