EdgeSymmetryBuilderSymmetryPlaneOptions Enumeration¶
NXOpen.Features.EdgeSymmetryBuilder.SymmetryPlaneOptions is an alias for NXOpen.Features.EdgeSymmetryBuilderSymmetryPlaneOptions
-
class
NXOpen.Features.
EdgeSymmetryBuilderSymmetryPlaneOptions
¶ Bases:
object
Symmetry plane options
Enum Members
Enum Member Enum Member Description YZ Uses YC-ZC plane as plane of symmetry XZ Uses XC-ZC plane as plane of symmetry XY Uses XC-YC plane as plane of symmetry Arbitrary Uses an arbitrary plane as plane of symmetry -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-