EdgeSymmetryBuilderMovementMethods Enumeration¶
NXOpen.Features.EdgeSymmetryBuilder.MovementMethods is an alias for NXOpen.Features.EdgeSymmetryBuilderMovementMethods
-
class
NXOpen.Features.
EdgeSymmetryBuilderMovementMethods
¶ Bases:
object
Matching method options
Enum Members
Enum Member Enum Member Description Normal Does a normal match Project Does a match by projecting poles corresponding to target edge of the surface WCS Does a match by moving poles along a WCS principal axis direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-