EdgeBlendBuilderRhotype Enumeration

NXOpen.Features.EdgeBlendBuilder.Rhotype is an alias for NXOpen.Features.EdgeBlendBuilderRhotype

class NXOpen.Features.EdgeBlendBuilderRhotype

Bases: object

This enum represents the rho type for conic section blend

Enum Members

Enum Member Enum Member Description
Relative
Absolute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.