EdgeBlendBuilderOverlap Enumeration¶
NXOpen.Features.EdgeBlendBuilder.Overlap is an alias for NXOpen.Features.EdgeBlendBuilderOverlap
-
class
NXOpen.Features.
EdgeBlendBuilderOverlap
¶ Bases:
object
This enum represents the Overlap resolution options for Edge Blend
Enum Members
Enum Member Enum Member Description MaintainAndIntersect Maintain Blend and Intersect DifferentConvexityRollOver If different convexity,roll over AnyConvexityRollOver Any convexity,roll over -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-