EdgeBlendBuilderFaceContinuity Enumeration

NXOpen.Features.EdgeBlendBuilder.FaceContinuity is an alias for NXOpen.Features.EdgeBlendBuilderFaceContinuity

class NXOpen.Features.EdgeBlendBuilderFaceContinuity

Bases: object

The Blend Face Continuity

Enum Members

Enum Member Enum Member Description
Tangent
Curvature
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.