EdgeBlendBuilderConic Enumeration

NXOpen.Features.EdgeBlendBuilder.Conic is an alias for NXOpen.Features.EdgeBlendBuilderConic

class NXOpen.Features.EdgeBlendBuilderConic

Bases: object

This enum represents the Conic option

Enum Members

Enum Member Enum Member Description
BoundaryPlusCenter
BoundaryPlusRho
CenterPlusRho
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.