DraftBuilderType Enumeration¶
NXOpen.Features.DraftBuilder.Type is an alias for NXOpen.Features.DraftBuilderType
-
class
NXOpen.Features.
DraftBuilderType
¶ Bases:
object
Describes the different Draft types
Enum Members
Enum Member Enum Member Description Face Face Draft type Edge From Edges type Tangent Tangent Draft type PartingEdge Draft with Parting Edges type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-