DraftBuilderMethod Enumeration¶
NXOpen.Features.DraftBuilder.Method is an alias for NXOpen.Features.DraftBuilderMethod
-
class
NXOpen.Features.
DraftBuilderMethod
¶ Bases:
object
Describes the Draft type as true draft or isocline draft.
Enum Members
Enum Member Enum Member Description Isocline Indicates use of isocline algorithm to create draft. Default value. TrueDraft Indicates use of true draft algorithm to create draft. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-