DraftBuilderDraftReferencesMethods Enumeration¶
NXOpen.Features.DraftBuilder.DraftReferencesMethods is an alias for NXOpen.Features.DraftBuilderDraftReferencesMethods
-
class
NXOpen.Features.
DraftBuilderDraftReferencesMethods
¶ Bases:
object
Describes the different Draft Methods in Draft References
Enum Members
Enum Member Enum Member Description StationaryFace Draft from stationary face. PartingFace Draft from stationary parting face. StationaryAndPartingFace Draft from stationary face to parting face. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-