DeleteFaceBuilderSetbackOptions Enumeration¶
NXOpen.Features.DeleteFaceBuilder.SetbackOptions is an alias for NXOpen.Features.DeleteFaceBuilderSetbackOptions
-
class
NXOpen.Features.
DeleteFaceBuilderSetbackOptions
¶ Bases:
object
Represents the set back options.
Enum Members
Enum Member Enum Member Description SelectedBlend Cap by setback along the selected blend. NeighborBlend Cap by setback along the neighbor of the selected blend. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-