DeleteFaceBuilderSelectTypes Enumeration¶
NXOpen.Features.DeleteFaceBuilder.SelectTypes is an alias for NXOpen.Features.DeleteFaceBuilderSelectTypes
-
class
NXOpen.Features.
DeleteFaceBuilderSelectTypes
¶ Bases:
object
Enumeration of select type, don’t use it until nx502
New in version NX5.0.2.
Enum Members
Enum Member Enum Member Description Face This stands for delete face type. Hole This stands for delete hole type. Blend This stands for delete blend type. FaceEdgeBlend This stands for delete notch blend type. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-