DatumPlaneBuilderUseArcLength Enumeration¶
NXOpen.Features.DatumPlaneBuilder.UseArcLength is an alias for NXOpen.Features.DatumPlaneBuilderUseArcLength
-
class
NXOpen.Features.
DatumPlaneBuilderUseArcLength
¶ Bases:
object
Specifies points for which arclength is to be used. Percentage of arclength is used for points for which arclength option is not selected. Specified for creation of datum plane using thru three points method.
Enum Members
Enum Member Enum Member Description NoPoint All points use percentage of arclength FirstPoint Only first point uses arclength SecondPoint Only second point uses arclength ThirdPoint Only third point uses arclength FirstAndSecondPoint Only first and second point use arclength FirstAndThirdPoint Only first and third point use arclength SecondAndThirdPoint Only second and third point use arclength AllPoints All points use arclength -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-