DatumPlaneBuilderFixedType Enumeration¶
NXOpen.Features.DatumPlaneBuilder.FixedType is an alias for NXOpen.Features.DatumPlaneBuilderFixedType
-
class
NXOpen.Features.
DatumPlaneBuilderFixedType
¶ Bases:
object
Specifies the fixed type datum plane going thru only one specific plane or thru all planes
Enum Members
Enum Member Enum Member Description All Fixed datum plane thru all planes Xy Fixed datum plane thru XY plane Yz Fixed datum plane thru YZ plane Zx Fixed datum plane thru ZX plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-