DatumPlaneBuilderConstraintType Enumeration¶
NXOpen.Features.DatumPlaneBuilder.ConstraintType is an alias for NXOpen.Features.DatumPlaneBuilderConstraintType
-
class
NXOpen.Features.
DatumPlaneBuilderConstraintType
¶ Bases:
object
Specifies different constraint types of selected geometries
Enum Members
Enum Member Enum Member Description Undefined Not defined Coincident Coincident constraint Parallel Parallel constraint Perpendicular Perpendicular constraint Center Center constraint Tangent Tangent constraint Distance Distance constraint Angle Angle constraint Frenet Frenet constraint -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-