DatumPlaneBuilderAlternateSolution Enumeration¶
NXOpen.Features.DatumPlaneBuilder.AlternateSolution is an alias for NXOpen.Features.DatumPlaneBuilderAlternateSolution
-
class
NXOpen.Features.
DatumPlaneBuilderAlternateSolution
¶ Bases:
object
Specifies the alternate solution for a datum plane using point on curve method
Enum Members
Enum Member Enum Member Description Tangent Indicates the datum plane as tangent to curve Normal Datum plane at normal to curve Binormal Datum plane at binormal to curve OppositeTangent Datum plane at opposite to tangent to curve OppositeNormal Datum plane at opposite to normal to curve OppositeBinormal Datum plane at opposite to binormal to curve Project This direction is calculated by projecting a point selected along a curve to a line, a datum axis, an edge of a solid, a planar face or a datum plane ProjectView Datum plane direction is calculated during creation based on the view plane. The datum plane normal is projected onto the view plane during creation time. The datum plane normal is maintained constant thereafter -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-