DatumAxisBuilderTypes Enumeration¶
NXOpen.Features.DatumAxisBuilder.Types is an alias for NXOpen.Features.DatumAxisBuilderTypes
-
class
NXOpen.Features.
DatumAxisBuilderTypes
¶ Bases:
object
New Datum Axis types in NX5
Enum Members
Enum Member Enum Member Description Inferred Inferred Intersection Datum axis at the intersection of objects CurveOrFaceAxis Datum axis at the curve or face axis OnCurveVector Datum axis at vector on curve XcAxis Datum axis thru X axis YcAxis Datum axis thru Y axis ZcAxis Datum axis thru Z axis PointAndDir Datum axis thru a point and parallel or perpendicular to direction TwoPoints Datum axis thru two point Fixed Indicate the datum axis is fixed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-