DatumAxisBuilderDirectionOrientations Enumeration¶
NXOpen.Features.DatumAxisBuilder.DirectionOrientations is an alias for NXOpen.Features.DatumAxisBuilderDirectionOrientations
-
class
NXOpen.Features.
DatumAxisBuilderDirectionOrientations
¶ Bases:
object
Two available direction orientations that the user can choose when the Datum Axis type is Point and Direction
Enum Members
Enum Member Enum Member Description ParallelToVector Orientation parallel to Direction PerpendicularToVector Orientation perpendicular to Direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-