DatumAxisBuilderCurveOrientations Enumeration¶
NXOpen.Features.DatumAxisBuilder.CurveOrientations is an alias for NXOpen.Features.DatumAxisBuilderCurveOrientations
-
class
NXOpen.Features.
DatumAxisBuilderCurveOrientations
¶ Bases:
object
Available orientations that the user can choose when the Datum Axis type is On Curve Vector
Enum Members
Enum Member Enum Member Description Tangent Orientation at tangent to curve Normal Orientation at normal to curve Binormal Orientation at binormal to curve PerpendicularToObject Orientation at perpendicular to object ParallelToObject Orientation at parallel to object -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-