CustomIntegerArrayAttribute Class¶
-
class
NXOpen.Features.
CustomIntegerArrayAttribute
¶ Bases:
NXOpen.Features.CustomAttribute
Represents a
Features.CustomIntegerArrayAttribute
classAn instance of this class can be obtained from
NXOpen.Features.CustomAttributeCollection.CreateCustomIntegerArrayAttribute()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the custom attribute name |
TypeValue | Returns the custom attribute type value |
Methods¶
Method | Description |
---|---|
AddProperty | The custom attribute add property |
Dispose | Frees the memory associated with this object. |
GetProperties | The custom attribute get all properties |
GetValues | Get the integer values in the attribute |
HasProperty | The custom attribute does property exist on attribute |
RemoveProperty | The custom attribute remove property |
SetValues | Set the integer values to the attribute |