CustomFeatureInformationEvent Class¶
-
class
NXOpen.Features.
CustomFeatureInformationEvent
¶ Bases:
NXOpen.Features.CustomFeatureEvent
Represents the event data for information callback for custom feature.
This class cannot be created
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ErrorCode | Returns or sets the error occured during the event |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetConstructionFeatures | The custom feature get construction features |
GetCustomFeature | Get the custom feature of the event |
GetNXObject | Returns the Solid body |
GetOutputFeatures | The output features created in post update event |
GetParasolidId | Get the Parasolid tag of Solid body |
SetInformation | The information about Custom Feature |