CustomFeatureDataCollection Class

class NXOpen.Features.CustomFeatureDataCollection

Bases: object

This class contains the factory method for creating custom feature data object.

To obtain an instance of this class, refer to NXOpen.Features.FeatureCollection

New in version NX11.0.0.

Methods

Method Description
CreateData Creates an Features.CustomFeatureData with parameters.

Method Detail

CreateData

CustomFeatureDataCollection.CreateData

Creates an Features.CustomFeatureData with parameters.

Signature CreateData(cfclass, attrs)

Parameters:
Returns:

custom feature data

Return type:

NXOpen.Features.CustomFeatureData

New in version NX11.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)