CustomExpressionArrayAttribute Class¶
-
class
NXOpen.Features.
CustomExpressionArrayAttribute
¶ Bases:
NXOpen.Features.CustomAttribute
Represents a
Features.CustomExpressionArrayAttribute
classAn instance of this class can be obtained from
NXOpen.Features.CustomAttributeCollection.CreateCustomExpressionArrayAttribute()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the custom attribute name |
TypeValue | Returns the custom attribute type value |
Methods¶
Method | Description |
---|---|
AddProperty | The custom attribute add property |
Dispose | Frees the memory associated with this object. |
GetProperties | The custom attribute get all properties |
GetValues | Get the expressions in the attribute |
HasProperty | The custom attribute does property exist on attribute |
RemoveProperty | The custom attribute remove property |
SetValues | Set the expressions in the attribute |
Method Detail¶
GetValues¶
-
CustomExpressionArrayAttribute.
GetValues
¶ Get the expressions in the attribute
Signature
GetValues()
Returns: Return type: list of NXOpen.Expression
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetValues¶
-
CustomExpressionArrayAttribute.
SetValues
¶ Set the expressions in the attribute
Signature
SetValues(expressionValues)
Parameters: expressionValues (list of NXOpen.Expression
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)