CustomAttributeType Enumeration¶
NXOpen.Features.CustomAttribute.Type is an alias for NXOpen.Features.CustomAttributeType
-
class
NXOpen.Features.
CustomAttributeType
¶ Bases:
object
Specifies custom attribute type.
Enum Members
Enum Member Enum Member Description Unknown Invalid or unknown. Expression Expression. ExpressionVla Expression variable length array. Tag Reference. TagVla Reference variable length array. Bool Bool. BoolVla Bool variable length array. Integer Integer. IntegerVla Integer variable length array. Double Double. DoubleVla Double variable length array. String String. StringVla String variable length array. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-