CopyPasteBuilderParentSelectOption Enumeration¶
NXOpen.Features.CopyPasteBuilder.ParentSelectOption is an alias for NXOpen.Features.CopyPasteBuilderParentSelectOption
-
class
NXOpen.Features.
CopyPasteBuilderParentSelectOption
¶ Bases:
object
Types of parent select option; Specifying smart object or selecting input for original parent
Enum Members
Enum Member Enum Member Description SmartObject Selecting input for the original parent. The creation method used for the input smart object for the copied feature may be selected from the creation methods that were available on the original feature. InputForOriginalParent Specifying smart object using the same creation method that was used in the original feature. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-