ConeBuilderTypes Enumeration¶
NXOpen.Features.ConeBuilder.Types is an alias for NXOpen.Features.ConeBuilderTypes
-
class
NXOpen.Features.
ConeBuilderTypes
¶ Bases:
object
Represents the Cone type
Enum Members
Enum Member Enum Member Description DiametersAndHeight Represents type of cone created by providing Diameters and Height DiametersAndHalfAngle Represents type of cone created by providing Diameters and Half Angle BaseDiameterHeightAndHalfAngle Represents type of cone created by providing Base Diameter, Height and Half Angle TopDiameterHeightAndHalfAngle Represents type of cone created by providing Top Diameter, Height and Half Angle TwoCoaxialArcs Represents type of cone created by providing Two Coaxial Arcs -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-