ColorFeatureGroupBuilderProcessType Enumeration¶
NXOpen.Features.ColorFeatureGroupBuilder.ProcessType is an alias for NXOpen.Features.ColorFeatureGroupBuilderProcessType
-
class
NXOpen.Features.
ColorFeatureGroupBuilderProcessType
¶ Bases:
object
set color for new features only or set color and apply to all members
Enum Members
Enum Member Enum Member Description NewFeatures set color for new features only AllMembers set color and apply to all members FirstLevelMembers set color and apply to first level members -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-