CircularBlendCurveBuilderCylinderRadiusOption Enumeration¶
NXOpen.Features.CircularBlendCurveBuilder.CylinderRadiusOption is an alias for NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
-
class
NXOpen.Features.
CircularBlendCurveBuilderCylinderRadiusOption
¶ Bases:
object
Represents the cylinder radius options
Enum Members
Enum Member Enum Member Description PointOnFirstCurve Radius by point on first curve PointOnSecondCurve Radius by point on second curve Value Radius by value -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-