BridgeCurveBuilderSurfaceDirectionTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.SurfaceDirectionTypes is an alias for NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes
-
class
NXOpen.Features.
BridgeCurveBuilderSurfaceDirectionTypes
¶ Bases:
object
This enum represents the direction type for input surfaces
Enum Members
Enum Member Enum Member Description Sectional bridge direction takes non-isoparametric direction of the base surface at the selected point IsoU bridge direction takes u-isoparametric direction of the base surface at the selected point IsoV bridge direction takes v-isoparametric direction of the base surface at the selected point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-