BridgeCurveBuilderShapeControlTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.ShapeControlTypes is an alias for NXOpen.Features.BridgeCurveBuilderShapeControlTypes
-
class
NXOpen.Features.
BridgeCurveBuilderShapeControlTypes
¶ Bases:
object
This enum represents the shape control types for the bridge curve
Enum Members
Enum Member Enum Member Description EndPoint end point conditions PeakPoint peak point conditions Conic conic parameter ShapeCurve shape curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-