BridgeCurveBuilderExShapeControlMethods Enumeration¶
NXOpen.Features.BridgeCurveBuilderEx.ShapeControlMethods is an alias for NXOpen.Features.BridgeCurveBuilderExShapeControlMethods
-
class
NXOpen.Features.
BridgeCurveBuilderExShapeControlMethods
¶ Bases:
object
Shape control methods
Enum Members
Enum Member Enum Member Description TangentMagnitude Shape using tangent magnitude at ends DepthSkew Shape using depth and skew value Conic Shape using rho value of a conic. Valid only when end sections are coplanar. TemplateCurve Shape by a template curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-