BridgeCurveBuilderExEndObjectTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilderEx.EndObjectTypes is an alias for NXOpen.Features.BridgeCurveBuilderExEndObjectTypes
-
class
NXOpen.Features.
BridgeCurveBuilderExEndObjectTypes
¶ Bases:
object
End object type
Enum Members
Enum Member Enum Member Description Section Section Object A point or face Datum A datum plane or axis for symmetric constraint Vector A vector representing a plane for symmetric constraint -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-