BridgeCurveBuilderEndObjectTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.EndObjectTypes is an alias for NXOpen.Features.BridgeCurveBuilderEndObjectTypes
-
class
NXOpen.Features.
BridgeCurveBuilderEndObjectTypes
¶ Bases:
object
This enum represents the current selected end object types for the bridge curve
Enum Members
Enum Member Enum Member Description Object allowed end object type except a vector object Vector vector object -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-