BridgeCurveBuilderCurveDirectionTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.CurveDirectionTypes is an alias for NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes
-
class
NXOpen.Features.
BridgeCurveBuilderCurveDirectionTypes
¶ Bases:
object
This enum represents the direction type for input curves
Enum Members
Enum Member Enum Member Description Tangent bridge direction takes the tangent direction of the base curve at the selected point Perpendicular bridge direction takes the direction that is perpendicular to the tangent direction of the base curve at the selected point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-